You are here: Tools > AKD into KAS > Workbench Reference > MOTOR.NAME

MOTOR.NAME

General Information

Type

NV Parameter

Description

Sets the motor name.

Units

N/A

Range

11 chars

Default Value

N/A

Data Type

String

See Also

N/A

Start Version

M_01-00-00-000

Description

This parameter is used to set the motor name.

Related Topics

Motor on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™