|
General Information |
|
|---|---|
|
Type |
NV Parameter |
|
Description |
|
|
Units |
rpm |
|
Range |
100 to 40,000 rpm |
|
Default Value |
3,000 rpm |
|
Data Type |
Integer |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
35A3h/0 |
M_01-00-00-000 |
Description
This parameter sets the maximum motor mechanical speed. The value 1.2 x MOTOR.VMAX becomes the overall overspeed fault threshold (VL.VFTHRESH) if it is less than the user overspeed fault threshold (VL.THRESH), and for MOTOR.TYPE = 6 if it is less than the motor back EMF overspeed threshold ((1.02 x 1000 x VBUS.OVFTHRESH) / (MOTOR.KE x sqrt(2))).
Related Topics
Motor | VL.THRESH on pg. 1 | VL.VFTHRESH on pg. 1
|
Copyright © 2015 Kollmorgen™ |
|