You are here: Tools > AKD into KAS > Workbench Reference > REC.DONE

REC.DONE

General Information

Type

R/O Parameter

Description

Checks whether or not the recorder has finished recording.

Units

N/A

Range

0 to 1

Default Value

N/A

Data Type

Integer

See Also

REC.ACTIVE, REC.OFF

Start Version

M_01-00-00-000

Description

REC.DONE indicates that the recorder has finished recording. This value is reset to 0 when the recorder trigger is set. The drive also resets this value when the recording has finished or when REC.OFF is executed.

Related Topics

Scope on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™