|
General Information |
|
|---|---|
|
Type |
R/O Parameter |
|
Description |
|
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
See Also |
|
|
Start Version |
M_01-00-00-000 |
Description
This command returns the list of recordable parameters. You can use a recordable parameter as an input to any of the recording channels.
Note that an internal address or a registered variable can be used as input to any of the channels in addition to the list.
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|