You are here: Tools > AKD into KAS > Workbench Reference > REC.TRIG

REC.TRIG

General Information

Type

Command

Description

Triggers the recorder.

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

See Also

REC.RETRIEVE, REC.OFF

Start Version

M_01-00-00-000

*For Profinet, write a value of 0 into the PNU to execute a command.

Description

REC.TRIG starts the trigger according to the trigger type defined by REC.TRIGTYPE.

REC.TRIG sets the value of REC.DONE to 0.

After calling REC.TRIG, the data that was recorded by previous recording is deleted and cannot be retrieved.

No REC parameters can be set after a call to REC.TRIG until the recorder has finished or until REC.OFF is executed.

Related Topics

Scope on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™