You are here: Tools > AKD into KAS > Workbench Reference > REC.TRIGPRMLIST

REC.TRIGPRMLIST

General Information

Type

R/O Parameter

Description

Reads the list of possible trigger parameters.

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

See Also

REC.TRIGPARAM

Start Version

M_01-00-00-000

Description

This command returns the list of trigger parameters. Each one of those parameters can serve as the trigger parameter (input to REC.TRIGPARAM).

Note that an internal address or a registered variable can be used as input to REC.TRIGPARAM in addition to the list that this parameter returns.

Related Topics

Scope on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™