You are here: Tools > AKD into KAS > Workbench Reference > REGEN.POWER

REGEN.POWER

General Information

Type

R/O parameter

Description

Reads regen resistor's calculated power.

Units

Watt

Range

N/A

Default Value

N/A

Data Type

Integer

See Also

N/A

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3416h/0

M_01-00-00-000

Description

This parameter reads regen resistor's calculated power, which is determined as follows:

(V2 / R) * DutyCycle

Related Topics

Regeneration

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™