You are here: Tools > AKD into KAS > Workbench Reference > REGEN.REXT

REGEN.REXT

General Information

Type

NV Parameter

Description

Sets the external, user-defined regen resistor resistance.

Units

Ω

Range

0 to 255 Ω

Default Value

0 Ω

Data Type

Integer

See Also

N/A

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

35C2h/0

M_01-00-00-000

Description

REGEN.REXT sets the external user-defined regen resistor resistance. This variable is needed for the regen resistor temperature estimation algorithm.

Related Topics

Regeneration

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™