You are here: Tools > AKD into KAS > Workbench Reference > SM.MOVE

SM.MOVE

General Information

Type

Command

Description

Starts the service motion.

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

See Also

SM.MODE

Start Version

M_01-00-00-000

*For Profinet, write a value of 0 into the PNU to execute a command.

Description

This command starts the service motion that has been selected by the SM.MODE parameter.

Related Topics

Service Motion on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™