You are here: Tools > AKD into KAS > Workbench Reference > TEMP.POWER1 to TEMP.POWER3

TEMP.POWER1 to TEMP.POWER3

General Information

Type

R/O Parameter

Description

Reads the temperature of the power board(s) temperature sensorA sensor is a type of transducer that converts one type of energy into another for various purposes including measurement or information transfer(s).

Units

Degrees Celsius

Range

-127 to 128

Default Value

N/A

Data Type

Integer

Start Version

M_01-09-00-000

Description

Reads the temperature of the power board(s) temperature sensor(s). Most AKDs have only one power board sensor which is read by TEMP.POWER1.

Related Topics

DRV.TEMPERATURES on pg. 1 | TEMP.CONTROL on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™