You are here: Tools > AKD into KAS > Workbench Reference > VBUS.OVFTHRESH

VBUS.OVFTHRESH

General Information

Type

R/O Parameter

Description

Reads the over voltage fault level.

Units

VDC

Range

0 to 900 VDC

Default Value

N/A

Data Type

Integer

See Also

VBUS.UVFTHRESH

Start Version

M_01-00-00-000

Description

VBUS.OVFTHRESH reads the over voltage fault level for the DC bus.

This value is read from the drive EEPROM and varies according to the drive type.

Related Topics

Regeneration on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™