You are here: Tools > AKD into KAS > Workbench Reference > VBUS.OVFWTHRESH

VBUS.OVWTHRESH

General Information

Type

NV Parameter

Description

Sets voltage level for over voltage warning.

Units

VDC

Range

0 to 900 VDC

Default Value

0 VDC (warning disabled)

Data Type

U16

See Also

N/A

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

518Eh/0

M_01-00-00-000

Description

If VBUS.VALUE value exceeds VBUS.OVWTHRESH, then a warning is generated. The warning is removed if the voltage returns to below 97% (1/32) of the overvoltage warning level.

Related Topics

Regeneration on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™