You are here: Tools > AKD into KAS > Workbench Reference > VBUS.UVWTHRESH

VBUS.UVWTHRESH

General Information

Type

NV Parameter

Description

Sets voltage level for undervoltage warning.

Units

VDC

Range

0 to 900 VDC

Default Value

10 volts above the default value of the under voltage fault threshold (VBUS.UVFTHRESH). The default value of VBUS.UVFTHRESH is hardware dependent.

Data Type

U16

See Also

VBUS.UVFTHRESH on pg. 1

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3495h/0

M_01-00-00-000

Description

If VBUS.VALUE value drops below VBUS.UVWTHRESH, then a warning is generated.

Related Topics

Regeneration on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™