You are here: Tools > AKD into KAS > Workbench Reference > VL.ARTYPE1 TO VL.ARTYPE4

VL.ARTYPE1 TO VL.ARTYPE4

General Information

Type

NV Parameter

Description

Indicates the method used to calculate BiQuad coefficients; active in opmodes 1 (velocity) and 2 (position) only.

Units

N/A

Range

0

Default Value

0

Data Type

U8

See Also

N/A

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Index/Subindex Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3405h/1

VL.ARTYPE1

M_01-02-00-000

3405h/2

VL.ARTYPE2

3405h/3

VL.ARTYPE3

3405h/4

VL.ARTYPE4

Description

These parameters indicate the method used to calculate the biquad coefficients VL.ARPFx, VL.ARPQx, VL.ARZFx, and VL.ARZQx. A value of 0 indicates that the coefficients are set directly. This parameter has no effect on the filter itself, but is only used to determine the original design parameters. Currently, only the value of 0 is supported.

Related Topics

Velocity Loop

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™