You are here: Tools > AKD into KAS > Workbench Reference > VL.FBUNFILTERED

VL.FBUNFILTERED

General Information

Type

R/O Parameter

Description

Reads the velocity feedback.

Units

Depends on UNIT.VROTARY or UNIT.VLINEAR, UNIT.ACCLINEAR

Rotary: rpm, rps, deg/s, (custom units)/s, rad/s

Linear: counts/s, mm/s, μm/s, (custom units)/s

Range

N/A

Default Value

N/A

Data Type

Float

See Also

VL.FB on pg. 1, VL.FBFILTER on pg. 1

Start Version

M_01-03-06-000

Description

VL.FBUNFILTERED reads the raw velocity feedback before any filters affect the value of this feedback.

Related Topics

Velocity Loop on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™