You are here: Tools > AKD into KAS > Workbench Reference > VL.KBUSFF

VL.KBUSFF

General Information

Type

R/W Parameter

Description

Sets the velocity loop acceleration feedforward gain value; active in opmodes 1 (velocity) and 2 (position) only.

Units

NA

Range

0.0 to 2.0

Default Value

0.0

Data Type

Float

See Also

VL.BUSFF on pg. 1

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3407h/3

M_01-00-00-000

Description

This parameter sets the gain for the acceleration feedforward (a scaled second derivative of the position command is added to the velocity command value).

The nominal feedforward value can be multiplied by this gain value.

This will have affect only when using position mode (DRV.OPMODE on pg. 1 = 2).

Related Topics

Velocity Loop

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™