You are here: Tools > AKD into KAS > Workbench Reference > WS.FREQ

WS.FREQ

General Information

Type

R/W

Description

Sets the sine frequency of excitation for WS.MODE 2.

Units

Hz

Range

0.01 - 8000

Default Value

10

Data Type

Float

Start Version

M_01-05-10-000

Description

This keyword sets the excitation frequency for Wake and Shake mode 2.

The default setting of 10Hz will work for almost all systems.

In cases where the load attached to the motor is much higher than the motor inertia (200:1) it may be necessary to lower the value of WS.FREQ.

Effects of lowering WS.FREQ:

Related Topics

WS.MODE on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™