IN : BOOL Process signal
ACK :
BOOL Acknowledge command
RST :
BOOL ResetNew start of the microprocessor command
Q : BOOL TRUE if alarm is active
QACK : BOOL TRUE if alarm is acknowledged
Combine this block with the LIM_ALRM block for managing analog alarms.
(* MyALARM is declared as an instance of ALARM_M function block *)
MyALARM (IN, ACK, RST);
Q := MyALARM.Q;
QACK := MyALARM.QACK;
(* MyALARM is declared as an instance of ALARM_M function block *)
Op1: CAL
MyALARM (IN, ACK, RST)
FFLD MyALARM.Q
ST"Structured text"
A high-level language that is block structured and syntactically resembles Pascal Q
FFLD MyALARM.QACK
ST
QACK
See also
|
Copyright © 2015 Kollmorgen™ |
|