You are here: Technical References > Programming Languages > PLC Standard Libraries > EXP / EXPL

EXP / EXPLPLCopen motion icon

FunctionA function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Calculates the natural exponential of the input.

Inputs

IN : REAL/LREAL   Real value

Outputs

Q : REAL/LREAL   Result: natural exponential of IN.

Remarks

In FFLD language, the operation is executed only if the input rung (EN) is TRUE. The output rung (ENO) keeps the same value as the input rung.

In IL"Instruction list" This is a low-level language and resembles assembly, the input must be loaded in the current result before calling the function.

ST Language

Q := EXP (IN);

FBD Language

FFLD Language

(* The function is executed only if EN is TRUE *)
(* ENO keeps the same value as EN *)
PowLd.gif (1506 octets)

IL Language:

Op1: LD"Ladder diagram"
Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them  IN
     EXP
     ST"Structured text" A high-level language that is block structured and syntactically resembles Pascal   Q    (* Q is: EXP (IN) *)

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™