You are here: Advanced Topics > Motion Bus and Fieldbuses > Fieldbus Editor > How to resolve errors

How to resolve errors

Device is not found

Error setting the IP configuration

CL-RPC Lookup

Timeout error

Other errors

Connect response error

Timeout error

Connect response error

Depending on the PNIO status error check, if the settings listed in the table below are set appropriate for your device.

PNIO Status Check the specified setting
1C010003 Slave\ObjectUUID (correct GDML file)
DB81010A Master\Activity timeout factor
DB81010B Master\Controller name
DB81010C Master\Controller name
DB810207 Master\RT-Class
DB81020A Master\Send clock factor
DB81020B Slave\Reduction ratio
DB81020C Slave\Phase
DB81020F Master\Watchdog factor
DB810210 Master\Watchdog factor
DB8103,* Slave\Module IDs,IOs
DB810407 Master\Alarm timeout
DB810408 Master\Alarm retries

Table 11-20: PNIO status error codes on connect and the related settings in the configuration

Module configuration is different

Writing parameterization error (with status 0XDF80*)

If your error could not be resolved using the hints above, update the firmware of your device and the GSDML file to the latest version and try again.

For further analyses record the PNIO communication using Wireshark.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™