You are here: Technical References > Programming Languages > PLC Standard Libraries > TMD

TMDPLCopen motion icon

Function BlockA function block groups an algorithm and a set of private data. It has inputs and outputs. - Down-counting stop watch.

Inputs

IN : BOOL   The time counts when this input is TRUE
RST : BOOL  Timer is reset to PT when this input is TRUE
PT : TIME   Programmed time

Outputs

Q : BOOL   Timer elapsed output signal
ET : TIME  Elapsed time

Time diagram

Remarks

The timer counts up when the IN input is TRUE. It stops when the programmed time is elapsed. The timer is reset when the RST input is TRUE. It is not reset when IN is false.

ST Language

(* MyTimer is a declared instance of TMD function block *)
MyTimer (IN, RST, PT);
Q := MyTimer.Q;
ET := MyTimer.ET;

FBD Language

FFLD Language

IL Language

(* MyTimer is a declared instance of TMD function block *)
Op1: CAL MyTimer (IN, RST, PT)
FFLD: MyTimer.Q
ST"Structured text" A high-level language that is block structured and syntactically resembles Pascal: Q
FFLD: MyTimer.ET
ST: ET

 

See also

TMU

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™