You are here: Technical References > Programming Languages > PLC Standard Libraries > ANY_TO_STRING

ANY_TO_STRINGPLCopen motion icon

Operator - Converts the input into string value.

Inputs

IN : ANY   Input value

Outputs

Q : STRING Value converted to string

Remarks

For BOOL input data types, the output is '1' or '0' for TRUE and FALSE respectively. For DINT, REAL or TIME input data types, the output is the string representation of the input number. It is a number of milliseconds for TIME inputs. In FFLD language, the conversion is executed only if the input rung (EN) is TRUE. The output rung (ENO) keeps the same value as the input rung. In IL"Instruction list" This is a low-level language and resembles assembly language, the ANY_TO_STRING function converts the current result.

ST Language

Q := ANY_TO_STRING (IN);

FBD Language

Any_To_StringFbd.gif (1300 octets)

FFLD Language

(* The conversion is executed only if EN is TRUE *)
(* ENO keeps the same value as EN *)
Any_To_StringLd.gif (1533 octets)

IL Language:

Op1: FFLD  IN
     ANY_TO_STRING
     ST  Q

See also

ANY_TO_BOOL   ANY_TO_SINT   ANY_TO_INT   ANY_TO_DINT   ANY_TO_LINT   ANY_TO_REAL   ANY_TO_LREAL   ANY_TO_TIME

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™