You are here: Technical References > Programming Languages > PLC Standard Libraries > CHAR

CHARPLCopen motion icon

FunctionA function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Builds a single character string

Inputs

CODE  : DINT ASCII code of the wished character

Outputs

Q : STRING     STRING containing only the specified character

Remarks

In FFLD language, the input rung (EN) enables the operation, and the output rung keeps the same value as the input rung. In IL"Instruction list" This is a low-level language and resembles assembly language, the input parameter (CODE) must be loaded in the current result before calling the function.

ST Language

Q := CHAR (CODE);

FBD Language

FFLD Language

(* The function is executed only if EN is TRUE *)
(* ENO is equal to EN *)

IL Language:

Op1: LD"Ladder diagram" Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them   CODE
     CHAR
     ST   Q

See also

ASCII

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™