You are here: Technical References > Programming Languages > PLC Advanced Libraries > CYCLESTOP

CycleStopPLCopen motion icon

FunctionA function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Sets the application in cycle stepping mode.

Inputs

IN : BOOL     Condition

Outputs

Q : BOOL      TRUE if performed

Remarks

This function turns the Virtual MachineThe complete assembly of all connected parts or devices, of which at least one is movable in "Cycle Stepping" mode. Restarting normal execution will be performed using the debugger.

The VM is set in "cycle stepping" mode only if the IN argument is TRUE.

The current main program and all possibly called sub-programs or UDFBs are normally performed up the end. Other programs of the cycle are not executed.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™