You are here: Technical References > Programming Languages > FFLD Language > FFLD Coils

FFLD Coils

Coils are basic graphic elements of the FFLD language. A coil is associated with a Boolean variable which is displayed above the graphic symbol. A coil performs a change of the associated variable according to the flow on its left-hand side.

Below are the six possible coil symbols:

Coils Description
boolVariable
   -( )-
Normal: the associated variable is forced to the value of the flow on the left of the coil.
boolVariable
   -(/)-
Negated: the associated variable is forced to the negation of the flow on the left of the coil.
boolVariable
   -(S)-

Set: the associated variable is forced to TRUE if the flow on the left is TRUE. (no action if the flow is FALSE)

boolVariable
   -(R)-

ResetNew start of the microprocessor: the associated variable is forced to FALSE if the flow on the left is TRUE. (no action if the rung state is FALSE)

boolVariable
   -(P)-
Positive transition: the associated variable is forced to TRUE if the flow on the left changes from FALSE to TRUE(and forced to FALSE in all other cases)
boolVariable
   -(N)-
Negative transition: the associated variable is forced to TRUE if the flow on the left changes from TRUE to FALSE(and forced to FALSE in all other cases)

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™