You are here: KAS IDE Reference > Create Programs > SFC Editor > Enter Macro-steps

Enter SFC macro-steps

A macro step is a special symbol that represents, within an SFC"Sequential function chart" It can be used to program processes that can be split into steps. The main components of SFC are: - Steps with associated actions - Transitions with associated logic conditions - Directed links between steps and transitions chart, a part of the chart that begins with a step and ends with a step. The body of the macro-step must be declared in the same program. The body of a macro-step begins with a special "begin" step with no link before, and ends with a special "end" step with no link after. The symbol of the macros step in the main chart has double horizontal lines.

Use the following buttons of the SFC toolbar to enter macro-steps:

Insert a macro-step
Insert the body of a macro-step

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™