You are here: Technical References > Programming Languages > SFC Language > Transitions

SFC Transitions

Transitions represent a condition that changes the program activity from a step to another.

The transition is marked by a small horizontal line that crosses a link drawn between the two steps.

The default direction for vertical links is from the top to the bottom

Transitions define the dynamic behavior of the SFC chart, according to the following rules:

Divergences

It is possible to link a step to several transitions and thus create a divergence. The divergence is represented by a horizontal line. Transitions after the divergence represent several possible changes in the situation of the program.

All conditions are considered as exclusive, according to a "left to right" priority order. It means that a transition is considered as FALSE if at least one of the transitions connected to the same divergence on its left side is TRUE.

Below is an example:


Transition 1 is crossed if:
step 1 is active
and Cond1 is TRUE

Transition 2 is crossed if:
step 1 is active
and Cond2 is TRUE
and Cond1 is FALSE

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™