You are here: Technical References > Programming Languages > PLC Standard Libraries > Sig_gen

Sig_GenPLCopen motion icon

Function BlockA function block groups an algorithm and a set of private data. It has inputs and outputs. - Generator of pseudo-analogical Signal

Inputs

RUN : BOOL Enabling command

PERIOD : TIME Signal period

MAXIMUM : DINT Maximum growth during the signal period

Outputs

This FB generates signals of the four following types:

FFLD Language

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™