Open topic with navigation
Confirm Connection with the Device
If you have more than one device connected to your network, then you can confirm that the new device is connected to the correct network as follows:
- A seven-segment LED display is located on the front of the device near the top. If you can see the display, then press the Blink button from the Overview screen in WorkBench and the device will flash the seven-segment display on and off.
- If it is difficult to see the display, then you can check the in the WorkBench list against the MAC address on the label of the device. The device is connected if the numbers displayed in WorkBench match the numbers printed on the label on the side of the device.
|
|
Copyright © 2015 Kollmorgen™
|
|
|
Open topic with navigation