Disconnected

When WorkBench is disconnected from a drive, no communication exists between your PCPersonal Computer and the drive.

The drive becomes disconnected because of one of the following conditions:

To restore communication:

  1. Clicking Connect will start communication with the drive. If WorkBench cannot find the drive, it will immediately return to the disconnected state.
  2. Pressing select will show a window where you can select a different drive you would like to use.
  3. Pressing delete will remove this drive from the navigation tree on the left hand side of the main window.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™