FunctionMLCNVInit

Description

Initializes a converter Pipe Block. FunctionA function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. block is automatically called if a Convertor Block is added to the Pipe Network, with the input mode (position or speed) entered in the Pipe Blocks Properties screen. The Converter block changes the incoming flow of speed or position values to continuous position output with no periodicity.

Arguments

Input

BlockID Description ID number of a created Pipe Block
  Data type DINT
  Range [-2147483648, 2147483648]
  Unit n/a
  Default
Mode Description 1 for Position mode, 2 for Speed mode. Determines the type of input to the Converter Object.
  Data type DINT
  Range [1, 2]
  Unit n/a
  Default

Output

Default (.Q)

Description Returns TRUE if the Convertor Pipe Block is initialized

See more details here

  Data type BOOL
  Unit n/a

Return Type

BOOL

Related Functions

MLBlkCreate

MLCNVConnect

Example

Structured Text

// Initiate a created convertor block named “CNV1”
CNV1 := MLBlkCreate( 'CNV1', 'CONVERTOR' );
MLCNVInit( CNV1, 1 );

Ladder Diagram

MLCNVInit: LD example

 

Function Block Diagram

MLCNVInit: FBD example

Go back to the top of the page [Top]

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™