MC_InitAxis
For more detail on how inputs and outputs work, refer to PLCopen Function Blocks - General Rules
|
En |
Description |
Request to initialize a PLCopen servo axis |
|
Data type |
BOOL |
|
|
Range |
0, 1 |
|
|
Unit |
n/a |
|
|
Default |
— |
|
|
AxisNumber |
Description |
Servo axis number |
|
Data type |
UINT |
|
|
Range |
[1,256] |
|
|
Unit |
none |
|
|
Default |
— |
|
|
VelocityLimit |
Description |
Velocity limit |
|
Data type |
LREAL |
|
|
Range |
— |
|
|
Unit |
User unit/sec |
|
|
Default |
— |
|
|
LowerLimit |
Description |
Lower position limit |
|
Data type |
LREAL |
|
|
Range |
— |
|
|
Unit |
User unit |
|
|
Default |
— |
|
|
UpperLimit |
Description |
Upper position limit |
|
Data type |
LREAL |
|
|
Range |
— |
|
|
Unit |
User unit |
|
|
Default |
— |
|
|
LimitControl |
Description |
Establishes how position limits are applied 0 = apply position limits 1 = ignore position limits 2 = ignore limits until referenced |
|
Data type |
UINT |
|
|
Range |
[0,2] |
|
|
Unit |
n/a |
|
|
Default |
— |
|
|
PosErrorLimit |
Description |
Position error limit – when the Position Error (command position – actual position) exceeds this value, an E-stop is generated |
|
Data type |
LREAL |
|
|
Range |
— |
|
|
Unit |
User unit |
|
|
Default |
— |
|
|
InPositionBand |
Description |
In-position bandwidthIn computer networking, bandwidth often refers to a data rate measured in bits/s, for example, network throughput. The reason for the connection of data rate with the term bandwidth is that the limit to the data rate of a physical communication link is related to its bandwidth in hertz – when the axis actual position is within this distance from its programmed endpoint, the axis is considered “in position” |
|
Data type |
LREAL |
|
|
Range |
— |
|
|
Unit |
User unit |
|
|
Default |
— |
|
OK |
Description |
Indicates the initialization is complete See more details here |
|
Data type |
BOOL |
(* MC_InitAxis ST"Structured text" A high-level language that is block structured and syntactically resembles Pascal example *)
AxisNumber1 := 1;
VelocityLimit1 := 10000; (*User unit/second*)
LowerPosLimit1 := 0;
UpperPosLimit1 := 0;
LimitControl1 := 0; (* Ignore lower and upper pos limit*)
PosErrorLimit1 := 10; (*User unit*)
InPosBand1 := 0;
MC_InitAxis(AxisNumber1, VelocityLimit1, LowerPosLimit1, UpperPosLimit1, LimitControl1, PosErrorLimit1, InPosBand1);
|
Copyright © 2015 Kollmorgen™ |
|