MC_Stop
MC_Stop cannot be aborted. This means that, while in Stopping state, no function block can command any motion on the axis. The axis remains in Stopping state until it reaches zero velocity and the Execute input is low. The application program can hold the axis in Stopping state even after it reaches zero velocity by leaving the Execute input high.
The example below shows the behavior of the combination of a MC_Stop FB with a MC_MoveVelocity FB.
FB1 MC_MoveVelocity reports an error indicating the busy MC_Stop command.
For more detail on how inputs and outputs work, refer to PLCopen Function Blocks - General Rules
| Execute | Description | Requests to stop the axis. It can be held high to prevent any other moves from being queued |
| Data type | BOOL | |
| Range | 0, 1 | |
| Unit | n/a | |
| Default | — | |
| Axis | Description | Name of a declared instance of the AXIS_REF library function. For more details, About Axis Name and Number |
| Data type | AXIS_REF | |
| Range | [1,256] | |
| Unit | n/a | |
| Default | — | |
| Deceleration | Description | Trapezoidal: Deceleration rate S-curve: Maximum deceleration |
| Data type | LREAL | |
| Range | — | |
| Unit | User unit/sec2 | |
| Default | — | |
| JerkIn physics, jerk is the rate of change of acceleration; more precisely, the derivative of acceleration with respect to time | Description | Trapezoidal: 0 S-curve: Constant jerkIn physics, jerk is the rate of change of acceleration; more precisely, the derivative of acceleration with respect to time |
| Data type | LREAL | |
| Range | — | |
| Unit | User unit/sec3 | |
| Default | — |
| Done | Description | Indicates the axis has reached zero velocity AND the Execute input is low |
| Data type | BOOL | |
| Busy | Description | High from the time the Execute input goes high until the axis reaches zero velocity AND the Execute input is low |
| Data type | BOOL | |
| Active | Description | High from the time the MC_Stop move becomes the active move, until the axis reaches zero velocity AND the Execute input is low |
| Data type | BOOL | |
| Error | Description | Indicates an invalid input was specified |
| Data type | BOOL | |
| ErrorID | Description | Indicates the error if Error output is set to TRUE |
| Data type | INT |
(* MC_Stop ST example *) Inst_MC_Stop( StopRequest , Axis1, 100.0, 100.0 ); //Inst_MC_Stop is an instance of MC_Stop function block StopComplete := Inst_MC_Stop.Done; //store the Done output into a user defined variable StopActive := Inst_MC_Stop.Active; //store the Active output into a user defined variable StopError := Inst_MC_Stop.Error; //store the Error output into a user defined variable
|
Copyright © 2015 Kollmorgen™ |
|