Output Status

The Done, Error, ErrorID and CommandAborted outputs are reset with the next rising edgeA rising edge is the transition of a digital signal from low to high. It is also called positive edge of Execute.

If an instance of a function block receives a new Execute before it finishes (as a series of commands on the same instance), the function block does not return any feedback, like Done or CommandAborted, for the previous action.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™