This feature is only available when you have chosen the DEBUG mode (for more details, Set the Compilation Options).
Pausing a program will not interrupt the current VM cycle. The current cycle will finish and execution will be paused before the beginning of the next VM cycle.
) or inactive (
).
and
) to indicate it has been reached in the code.Breakpoints can significantly increase the PLC"Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events cycle time execution. This is due to the fact that the VM must evaluate the breakpoint condition at every cycle.

The breakpoints are not activated synchronously but in a reasonable time.
|
Copyright © 2015 Kollmorgen™ |
|