Distributed Clock tab

The contents of this tab allow you to change settings related to the Distributed ClockClock signal for all Kollmorgen and third-party devices (both discovered and manually added).

Element Description
Distributed Clock Profile Select the Distributed Clock (DC) operation mode. These modes cannot be edited.
Master Cycle Time Base interval in microseconds, which will be used by the master. This is changed and automatically updated by changing the Cycle Time value on the EtherCAT Master Settings tab.
Sync Unit 0

Cycle Time:

  • Sync Unit Cycle: Unit is synchronized relative to the Master Cycle Time
  • User defined: Unit has its own interval

Shift Time:

  • Unit is adjusted by the shift time
Sync Unit 1

Cycle Time:

  • Sync Unit Cycle: Unit is synchronized relative to the Master Cycle Time
  • Sync 1 Cycle: Unit is synchronized relative to the First Sync Unit
  • User defined: Unit has its own interval

Shift Time:

  • Unit is adjusted by the shift time

Oversampling devices

Some EtherCAT devices have oversampling features. An oversampling device is typically able to record (input) or provide (output) signals at a higher rate than the EtherCAT cycle time. This rate is called the oversampling factor. For example, with an oversampling factor of 10 and an EtherCAT cycle time of 1ms (1Khz), an input device can record values every 100µs (1000 divided by 10).

Oversampling devices have as many PDO objects in their cyclic frames as the oversampling factor in order to achieve the higher rate. Each of these PDO objects corresponds to one sample. For example, an output device with an oversampling factor of 4 will typically have 4 PDO objects: Output 1, Output 2, Output 3 and Output 4.

The oversampling factor is tied to the Distributed Clock Profile. A warning is displayed next to the DC profile selection box in the Distributed Clocks tab when a device has oversampling features, as seen below.

Figure 4-115: Example of a device with oversampling.

Changing the Distributed Clock Profile will automatically change the PDO selection. All PDOs corresponding to the selected Distributed Clock Profile and its according oversampling factor will be selected. These maps will be discarded if one or several PLC"Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events variables were mapped to a PDO that is no longer selected.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™