They do not apply to actions in an SFC"Sequential function chart" It can be used to program processes that can be split into steps. The main components of SFC are: - Steps with associated actions - Transitions with associated logic conditions - Directed links between steps and transitions step.
Conditional compiling coloring
Parts of conditional compiling code (declared with #ifdef pragmas) that are not validated are grayed
Commenting the CONDITION changes the active part of the program
Save your project to have the code with the correct colors.
Auto-indentation
Lines are automatically indented on the left when you enter structured ST statements
|
Copyright © 2015 Kollmorgen™ |
|