The elements that you can print are:
You can either print one specific program or all the project (PLC, Motion, Dictionary variables)
This dialog enables you to define the following settings:
Page Setup tab
These settings are not applicable when printing a project.
Margin and Header/Footer tab
If you specify new margins or header/footer for a program, it affects the entire project when printed.
Special items can be inserted into the header/footer string as {@item}. They are converted to the correct format on printing or for print preview.
About the Filename field:
If an SFC level 2 program is being printed, the filename contains the SFC program name, Step or Transition number and the action tab name (e.g. Main, GS3, P1).
All the settings defined in the Page Setup are saved within your project and are applied to each printed program.
This dialog box also contains two buttons:
This dialog enables you to:
To print an SFC level 2 program, open it in the SFC editor and click the Print icon
(Ctrl + P)
This dialog box enables you to display a printout on the screen so you can see how it looks before printing.
A Print Project dialog displays all the items that are printable. Then you can select those you want to include in your output and click OK.
Selecting an SFC program prints the SFC chart as well as SFC level 2 programs.
Automatic scaling is applied for best readability.
|
Copyright © 2015 Kollmorgen™ |
|