Design The KVB Panel

Add Object

You can drag-and-drop predefined objects from the library to the screen. The library is located in the Home tab of Kollmorgen Visualization Builder.

Customize Object

Select an object and click the General tab to customize:

Map Variable to the Object

In the General tab, you can set the Variable or Tag that maps to the current object in the Tag/Security section.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™