Log Messages

Log Messages

Figure 3-8: Log Messages

Log messages are displayed on two tabs, Local log and Controller log.

Based on the configuration settings (see call out ), only messages that are recorded and that match the filter are displayed.

Every log message in the table widget has the following information:

Field

Description

Time

Time when the log was recorded with the format:
DD-MMMM-YY hh:mm:ss (millisecond)

 

Source

Identifies a software or hardware component issuing the messages. Each source is configured with a specific Level.

 

Level

Each message has one of the following levels with importance in ascending order:
DEBUG > INFO > WARNING > ERROR > CRITICAL

 

Message

Text of the message issued from the source

 

Table 3-22: Log Messages - List of Fields

The table contains a contextual menu (see call out ) with the following commands:

Command

Description

DisableRemoval of the ENABLE signal. Disables power stage./
EnableEnable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set. Both are required for enabling the drive.

You can stop the log recording at any time, so that no more messages are added

 

Clear

Empty the list by erasing all the messages already recorded

 

Copy

Copy the text of the selected messages to the clipboard (you can perform multi-selection with the Ctrl or Shift keys)

 

Save As

Save all the messages in a log file

 

Select All

Select all the messages that are displayed in the table

 

Table 3-23: Log Messages - List of Buttons

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™