All the structures within the entire system project are grouped as follows:
|
Description |
|
|
EtherCATCode |
List all the devices as PLC"Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events variables so you can use their names in FBs instance • The devices are displayed under the EtherCAT node in the Project Explorer (see call out • The same devices are also displayed as PLC variables in the Dictionary • You can use them in your PLC programs with a drag-and-drop operation
|
|
PNCode |
List all the variables related to the specific Pipe Network Code |
|
ProfilesCode |
List all the variables related to the specific profiles |
|
PLCopenCode |
List all the variables related to the specific PLCopenA vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML Code |
|
List the variables related to a specific UDFB |
|
Copyright © 2015 Kollmorgen™ |
|