AIN.DEADBANDMODE

General Information

Type

NV Parameter

Description

Sets the analog input deadband mode.

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

See Also

AIN.DEADBAND

Start Version

M_01-03-06-000

Variants Supported

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

5251h/0

M_01-03-06-000

Description

When AIN.DEADBANDMODE is set to 0, and the value of the analog input is less than the value of AIN.DEADBAND, the analog command will be 0. When the analog input is greater or equal to the AIN.DEADBAND, then the analog command will be generated using the scaling specified.

When AIN.DEADBANDMODE is set to 1, the analog command is 0 if the input is less than the deadband value. When the input is greater than the deadband, the output is equal to (Input - Deadband) * Scaling. Below are illustrations of this behavior.

Related Topics

Analog Input

Block Diagram for Position/Velocity Loop

AIN.DEADBAND

 

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™