AIN.ZERO

General Information

Type

Command

Description

Zeroes the analog input signal.

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

See Also

AIN.VALUE , AIN.OFFSET

Start Version

M_01-00-00-000

Variants Supported

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

N/A

M_01-00-00-000

*For Profinet, write a value of 0 into the PNU to execute a command.

Description

AIN.ZERO causes the drive to zero the analog input signal (AIN.VALUE ). You may need to execute this command more than once to achieve zero offset, and AIN.OFFSET is modified in this process.

Related Topics

Analog Input

AIN.VALUE | AIN.OFFSET

Block Diagram for Position/Velocity Loop

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™