CMPx.MODE

General Information

Type

NV Parameter

Description

Sets the mode for a Compare setpointSetpoint is the target value that an automatic control system, for example PID controller, will aim to reach.

Units

None

Range

Argument 1: 0 to 7

Argument 2: 0 (Single-shot) or 1 (Continuous)

Default Value

1 (Continuous)

Data Type

Argument 1: Integer

Argument 2: Integer

Start Version

M_01-13-00-000

Compare functionality is supported on hardware revisions D, DB, DA, and higher depending on the drive type. Check the label on the side of the drive to ensure the AKD meets one of the following requirements.

AKD Type Hardware Revision Supported
AKD Revision D or higher
PDMM Revision DB or higher
AKD-T-IC"Integrated Circuits" Miniaturized electronic circuits (consisting mainly of semiconductor devices, as well as passive components) that have been manufactured in the surface of a thin substrate of semiconductor material Revision DA or higher
FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Index/Subindex Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

34ADh/1 CMP0.MODE 0 M_01-13-00-000
34AAh/2 CMP0.MODE 1
34AAh/3 CMP0.MODE 2
34AAh/4 CMP0.MODE 3
34AAh/5 CMP0.MODE 4
34AAh/6 CMP0.MODE 5
34AAh/7 CMP0.MODE 6
34AAh/8 CMP0.MODE 7

34BDh/1

CMP1.MODE 0

34BAh/2

CMP1.MODE 1

34BAh/3

CMP1.MODE 2

34BAh/4

CMP1.MODE 3

34BAh/5

CMP1.MODE 4

34BAh/6

CMP1.MODE 5

34BAh/7

CMP1.MODE 6

34BAh/8

CMP1.MODE 7

Description

This keyword sets the mode for a Compare setpoint to either single-shot or continuous. Single-shot automatically disarms the setpoint after a pulse is generated. Continuous mode will keep the setpoint armed after a pulse has been generated.

Example

The following example sets the mode for setpoint 3 to single-shot.

-->CMP1.MODE 7 0

Related Topics

Compare Engines

CMPx.SETPOINT

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™