DRV.DISMODE

General Information

Type

NV Parameter

Description

Selects among disable immediately or stop and then disable options.

Units

N/A

Range

0 to 3

Default Value

0

Data Type

Integer

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

35FFh/0

M_01-00-00-000

Description

DRV.DISMODE sets the drive reaction to a DRV.DIS (software disable) or fieldbus command.

Value Behavior

0

DisableRemoval of the ENABLE signal. Disables power stage. axis immediately. If MOTOR.BRAKEIMM = 1, the brake is applied as soon as the power stage disables.

1

Use dynamic brake to ramp down. The drive remains in the dynamic brake state after the motor has stopped. The drive is disabled in the sense that it does not close the control loop and cannot perform a motion, but PWM stays active.

2

Use a controlled stop to ramp down and then disable the drive.

3

Use a controlled stop to ramp down, and then use dynamic brake. The drive remains in the dynamic brake state after the motor has stopped. The drive is disabled in the sense that it does not close the control loop and cannot perform a motion, but PWM stays active.

Related Topics

Enable/Disable

Controlled Stop

CS Parameters

Dynamic Braking

DRV.DBILIMIT , DRV.DISTO , CS.VTHRESH

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™