DRV.EMUESTEPCMDPOUT

General Information

Type

R/W

Description

Scaling factor (denominator) for the command DRV.EMUESTEPCMD.

Units

N/A

Range

-65536 to 65536

Default Value

65536

Data Type

Integer

Start Version

M_01-14-03-000

Description

This parameter is the denominator in the scaling factor for DRV.EMUSTEPCMD.

The internal stepper command is calculated as follows:

Related Topics

Stepper Control and EEOs over fieldbus

DRV.EMUESTEPCMD | DRV.EMUESTEPCMDPIN

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™