|
General Information |
|
|---|---|
|
Type |
R/W Parameter |
|
Description |
|
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
0 |
|
Data Type |
Boolean |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
5080h/0 |
M_01-00-00-000 |
Description
DRV. ENDEFAULT sets the default state of the software enable on power up for drives without fieldbusesA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design (DRV.CMDSOURCE other than 1).
It is recommended to not use this parameter with a BASIC program (keep DRV.ENDEFAULT = 0 / default value). Instead set DRV.SWENABLE = 1 at the beginning of the BASIC program.
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|