DRV.FAULTDISPLAYMODE

General Information

Type

NV Parameter

Description

Sets the fault display mode.

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Start Version

M_01-13-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Index/Subindex Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

53C7h

M_01-13-00-000

Description

DRV.FAULTDISPLAYMODE sets the LED display behavior when faults are present.

Value Description
0 Only the highest priority fault is displayed.
1 All faults displayed.

Related Topics

DRV.CLRFAULTS , DRV.FAULTHIST, DRV.CLRFAULTHIST

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™