DRV.HANDWHEEL

General Information

Type

R/O Parameter

Description

Reads the EEO input value.

Units

1/4,294,967,296 rev

Range

0 to 4,294,967,295 rev

Default Value

0 rev

Data Type

Integer

See Also

DRV.EMUERES , DRV.EMUEMODE

Start Version

End Version

M_01-00-00-000

M_01-03-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

2050h/0

M_01-00-00-000

Description

When the EEO is selected as an input (DRV.EMUEMODE =3,4,5), this parameter reads the EEO value (where 4,294,967,296 is a full revolution, then the value rolls over). DRV.EMUERES defines the how many counts constitute a revolution on the EEO. This parameter represents the feedback 2 positions when feedback 2 is configured to be active.

When secondary feedback is selected (DRV.EMUEMODE is 0 and FB2.SOURCE = 1 (X9), or FB2.SOURCE = 2 (X7)), this parameter represents the secondary feedback position (where 4,294,967,296 is a full revolution, then the value rolls over). FB2.ENCRES defines how many counts define a revolution for the secondary feedback.

Related Topics

 

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™