|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3506h/0 |
M_01-03-00-000 |
Description
This parameter selects the action that the hardware enable digital input will perform.
0 = The rising edgeA rising edge is the transition of a digital signal from low to high. It is also called positive edge of the hardware enable will clear the drive faults.
1 = The rising edge of the hardware enable will not clear the drive faults.
The high/low state of the hardware enable is always used to control the active enable state of the drive.
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|